:DISPlay:JITTer:OJITter:ECATegory

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Output Jitter

Command Syntax

:DISPlay:JITTer:OJITter:ECATegory {ALL | C03 | R01 | R02 | R03 | R12 | R13 | R23 | F10 | F20 | F30 | F21 | F31 | F32}

Query Syntax

:DISPlay:JITTer:OJITter:ECATegory?

Query Response

 {ALL | C03 | R01 | R02 | R03 | R12 | R13 | R23 | F10 | F20 | F30 | F21 | F31 | F32}

Description

Selects the type of waveform edge (edge category) on which to construct the displayed Output Jitter Histogram graph. This histogram is displayed in Jitter mode when 12-Edge Output Jitter measurements on PAM4 waveforms is activated using the :MEASure:JITTer:OJITter:STATe command.

Command arguments select a specific waveform edge for the histogram: rising or falling. Arguments for rising edges start with the letter R. Arguments for falling edges start with the letter F. For example, the argument R23 selects the rising edge from the waveform level 2 to level 3. The default argument ALL selects all edges. You can also select to have a composite of Rising (R03) and Falling (F30) edges using the C03 argument.

The following table shows the position of related measurements (by command argument) on the Output Jitter panel.

Command Argument Versus Selected Edge
Starting
Level
Destination Level
To L0 To L1 To L2 To L3
From L3 F30 F31 F32
From L2 F20 F21 R23
From L1 F10 R12 R13
From L0 R01 R02 R03

This command does not affect the edge-type selections that are used to return specific measurements made with the following commands:

Revision A.07.00 added the C03 argument.

Requires FlexDCA revision A.05.70 and above.