:MEASure:JITTer:OJITter:SJNU

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Output Jitter

Command Syntax

:MEASure:JITTer:OJITter:SJNU {J1U | J2U | J3U | J4U | J5U | J6U | J7U | J8U | J9U}

Query Syntax

:MEASure:JITTer:OJITter:SJNU?

Query Response

 {J1U | J2U | J3U | J4U | J5U | J6U | J7U | J8U | J9U}

Description

For an IEEE 12-Edge Output Jitter measurement, selects an output jitter measurements that are based on a specific probability as listed in the following table.

Arguments for Jitter Measurement Probabilities
Argument Probability
J9U 10–9
J8U 10–8
J7U 10–7
J6U 10–6
J5U 10–5
J4U 10–4
J3U 10–3
J2U 10–2
J1U 10–1

To select the waveform's edge (edge category) for the measurement, use the :MEASure:JITTer:OJITter:JNU:ECATegory command. To return the measurement, use the :MEASure:JITTer:OJITter:JNU? query. The measurement result is always for a specified type and edge category.

This command is equivalent to the Select Jnu Type field in the Jitter Measurements tab of the Jitter Mode Measurement Setup dialog. Use the :DISPlay:JITTer:OJITter:ECATegory command to select the type of waveform edge (edge category) on which to construct the displayed Output Jitter Histogram graph.

With revision A.06.80, added the J6U, J7U, J8U, and J9U waveform edge categories.

Requires FlexDCA revision A.06.00 and above.

Related Commands