:DISK:DWIZard:POJitter:SDATa
Instrument:
N1000A
DCA-M
Meas. mode:
Jitter
Flex Apps:
FlexDCA
Command Syntax
:DISK:DWIZard:POJitter:SDATa {ON | OFF | 1 | 0}
Query Syntax
:DISK:DWIZard:POJitter:SDATa?
Query Response
{ON | OFF | 1 | 0}
Description
When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the results for Jitter mode's Phase-Only Jitter measurements for PAM4 waveforms. These measurements are activated by the :MEASure:JITTer:POJitter:STATe command. The command arguments are:
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
The following two files are added to the Documentation Wizard zip file:
- An ASCII CSV file of the Timing Jitter panel measurement results including table labels (Timing Jitter Window Results.csv).
- A screen capture of the Timing Jitter panel measurement results (Timing Jitter Window Screen Capture.png), as shown in the following figure.
Requires FlexDCA revision A.08.30 and above.
Example
:MEASure:JITTer:STATe ON :MEASure:JITTer:POJitter:STATe ON :DISK:DWIZard:FNAMe "%USER_DATA_DIR%\Documentation Results\DocResults_POJ.zip" :DISK:DWIZard:POJitter:SDATa ON :DISK:DWIZard:SSCReen OFF :DISK:DWIZard:SSETup OFF :DISK:DWIZard:JGRaphs:SDATa OFF :DISK:DWIZard:TIME1:SDATa OFF :DISK:DWIZard:SSINfo OFF :DISK:DWIZard:SAVe;*OPC?