:SYSTem:AUToscale
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SYSTem:AUToscale
Description
Performs an Auto Scale. There is no query form of this command. If the Auto Scale is unsuccessful, one or more errors are placed in the last-in first-out error-message buffer. Use the :SYSTem:ERRor:NEXT? and :SYSTem:ERRor:COUNT? queries to determine if an error has occured and the cause of any errors. The following errors can be reported:
- 143, "Instrument Error;Autoscale: No valid sources are turned on."
- 144, "Instrument Error;Autoscale: Could not detect data rate."
- 144, "Instrument Error;Autoscale: Unable to detect reference clock frequency."
Before using Auto Scale, turn on at least one channel and ensure a valid signal and trigger source is connected. During an Auto Scale, the following tasks are performed:
- Scales the waveform vertically and horizontally for all the input channels that are turned on.
- Adjusts the trigger level in Oscilloscope, Eye/Mask, or Jitter Mode.
- Sets trigger bandwidth.
- Sets the horizontal scale and position of the lowest numbered channel turned on.
- If multiple eye diagrams are displayed software delay is used to align the eye diagrams. However, the following conditions must be true:
- Option 500, Productivity Package License, is installed,
- Rapid Eye is turned on (
:ACQuire:REYE), and - Rapid Eye align is specified (
:ACQuire:REYE:ALIGn).
To autoscale only the vertical or only the horizontal axis, use the :SYSTem:AUToscale:VERTical or :SYSTem:AUToscale:HORizontal child commands.