:MEASure:JSAMemory:DJ:STATus?
Instrument:
N1000A
N107x-JSA
N1060A-JSA
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
L-SNT
Waveforms:
NRZ
PAM4
Query Syntax
:MEASure:JSAMemory:DJ:STATus?
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
- QUES
- The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.
Description
Queries the status of the JSA deterministic jitter DJ (rms) measurement. Use the :STATus:REASon? child query to determine the reason for an invalid or questionable measurement. Additional information about the failure may be available using the :STATus:DETails? child query.
Requires FlexDCA revision A.04.00 and above.