:MEASure:JSAMemory:DJ:STATus:REASon?

Instrument:
N1000A
N107x-JSA
N1060A-JSA
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
L-SNT
Waveforms:
NRZ
PAM4

Query Syntax

:MEASure:JSAMemory:DJ:STATus:REASon?

Query Response

Refer to the table "Possible Common :STATus:REASon? Query Responses".

Description

Returns a string that explains the reason for a failed :CRECovery:DJ measurement. If the measurement was successful, a null string is returned.

Additional information about the failure may be available using the :STATus:DETails? sibling query. Use the :CRECovery:DJ:STATus? parent query to determine if the measurement has failed.

Requires FlexDCA revision A.04.00 and above.