:MEASure:JSAMemory:DJ:STATus:DETails?
Instrument:
N1000A
N107x-JSA
N1060A-JSA
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
L-SNT
Waveforms:
NRZ
PAM4
Query Syntax
:MEASure:JSAMemory:DJ:STATus:DETails?
Description
Returns a string that may provide additional details for a failed :JSAMemory:DJ measurement. If the measurement was successful, a null string is returned.
For a basic description of a measurement failure, use the :STATus:REASon? sibling query. Use the :STATus? parent query to determine if the measurement has failed.
Requires FlexDCA revision A.04.00 and above.