:MEASure:JSAMemory:DJ?

Instrument:
N1000A
N107x-JSA
N1060A-JSA
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
L-SNT
Waveforms:
NRZ
PAM4

Query Syntax

:MEASure:JSAMemory:DJ?

Description

Queries the JSA DJ (rms) measurement, which is a band-limited Deterministic Jitter measurement. Specify the integration limits using the :CRECovery:JSANalysis:INTegrate:F command.

Requires an N1060A or N107x-series clock recovery module with an L-RND or L-SNT license for Jitter Spectrum Analysis and SW Clock Recovery Emulation .

Requires FlexDCA revision A.04.00 and above.

Example Command Sequence

:MEASure:CRECovery:DJ?

Measurement Ready?

To confirm that the measurement is ready to read, you can query the measurement's status:

if ('CORR' in Flex.query(':STATus?')):
	measurement = Flex.query('?')

If averaging is turned on (:ACQuire:AVERaging), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:ECOunt?) versus the number of measurement sweeps that have occurred (:COUNt?). The technique uses the :COUNt? common measurement query. For example,

if (Flex.query(':COUNt?') >= Flex.query(':ACQuire:ECOUNt?')):
	measurement = Flex.query('?')

You can also use an acquisition limit lest to test that a number of waveform samples, or pattern acquisitions have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.

Common Measurement Child Queries

This command supports the use of the following common measurement queries: :LOCation?, :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.