:MEASure:LLINe:LINE:MLOCation?
Query Syntax
:MEASure:LLINeN:LINEM:MLOCation?
Where N identifies one of 64 {1:64} possible limit line tests. For example, :LLINe23.
Where M identifies one of 16 {1:16} possible limit lines.
Description
Queries the location in time of the data point where the pass/fail margin is reported for a specific limit line. The returned time value is the same value that is shown in the Details dialog which is displayed from the Limit Lines panel. To return the pass/fail margin, use the :MEASuer:LLINe:LINE:MARGin? query. To return the total number of failed data points (which is zero for positive margins) use the :MEASure:LLINe:LINE:FPOints? query. To load and display a Limit Line Test, use the :LLINe:DISPlay command.
Only displayed data points are analyzed. For example, if you zoom in on the waveform so that a portion of the Limit Line Test is off screen, any failed data point that exists off screen will not be analyzed.
Requires FlexDCA revision A.04.50 and above.