:MEASure:LLINe:MARGin:STATus:REASon?
Meas. mode:
Scope
TDR
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:MEASure:LLINeN:MARGin:STATus:REASon?
Where N identifies one of 64 {1:64} possible limit line tests. For example, :LLINe23.
Query Response
Refer to the table "Possible Common :STATus:REASon? Query Responses".
Description
Returns a string that explains the reason for a failed :LLINe:MARGin measurement. If the measurement was successful, a null string is returned. Use the :LLINe:MARGin:STATus? parent query to determine if the measurement has failed.
Requires FlexDCA revision A.04.50 and above.