:MEASure:LTESt:ACQuire:COUNt?
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:MEASure:LTESt:ACQuire:COUNt?
Description
Use this query to return the current waveforms, patterns, or samples counted when a waveform, pattern, or samples acquisition limit test is enabled (:LTESt:ACQuire:STATe command). This is the count that is shown in FlexDCA's upper-right corner. The following :LTESt sybsystem commands are used to specify the count number:
The current count can be helpful in instances where aqcuiring the specified number of waveforms, patterns, or samples takes some time and you need to estimate the completion time.
Requires FlexDCA revision A.05.30 and above.