:LTESt:ACQuire:STATe
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:ACQuire:STATe {ON | OFF | 1 | 0}
Query Syntax
:LTESt:ACQuire:STATe?
Query Response
{1 | 0}
Description
Enables acquisition limit testing. The actual test is started by placing FlexDCA in run mode (:ACQuire:RUN). You must use the :ACQuire:RUN command to start continuous sweeps and so begin the test. During the limit test, use the :MEASure:LTESt:ACQuire:COUNt? query to return the current count of patterns, samples, or waveforms. When the acquisition limit test completes, FlexDCA acquisition is automatically stopped (:ACQuire:STOP). Upon completion of the limit test, disable limit testing (:LTESt:ACQuire:STATe OFF).
Example Command Sequence
The following example shows how to create an acquisition limit test that runs until 100 waveforms have been acquired.
:ACQuire:SINGle // Stop waveform acquisition. :LTESt:ACQuire:CTYPe WAVeforms // Create test based on acquisition to waveforms. :LTESt:ACQuire:CTYPe:WAVeforms 100 // Stop test after 100 waveforms acquired. :LTESt:ACQuire:SWAVeform:CHAN1B:STATe MEMory // Save channel 1B to waveform memory. :LTESt:ACQuire:SWAVeform:CHAN1B:WMEMory WMEMory2 // Select waveform memory 2. :LTESt:ACQuire:SIMage:STATe ON // Save screen image. :LTESt:ACQuire:SIMage:INVert ON // Invert colors on screen image. :LTESt:ACQuire:SIMage:WINDow TIME1 // Capture only waveform instead of entire display. :LTESt:ACQuire:SIMage:FNAMe "C:\Users\me\Documents\Keysight\FlexDCA\Screen Images\my test.jpg" // Create this image file. :LTESt:ACQuire:STATe ON // Turn limit test on. :ACQuire:RUN // Start waveform acquisition. *OPC? // Wait for test completion. :LTESt:ACQuire:STATe OFF