Limit Test Results
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Limit testing allows you to stop data acquisition based on limits placed on one of the four types of events:
- Acquisitions
- Measurements
- Limit-Line-Tests
- Masks
When the specified limit conditions are met, the active tasks stop and, if defined, a reporting action is taken for each limit test. The following table shows the availability of each type of limit test according to instrument modes. You can run one or more limit tests at a time. As soon as the limit conditions for one of the tests is met, data acquisition and all tests stop. To reset any of the limit tests, click Clear on the menu bar or change any of the following parameters: vertical scale, offset, horizontal position, horizontal scale, trigger settings, acquisition record length, or averaging.
| Type of Limit Test | Instrument Mode | |||
|---|---|---|---|---|
| Oscilloscope | Eye/Mask | TDR/TDT | Jitter | |
| Acquisition Limits | ♦ | ♦ | ♦ | ♦ |
| Measurement Limits | ♦ | ♦ | ♦ | ♦ |
| Limit-Line-Test Limits | ♦ | ♦ | ||
| Mask-Test Limits | ♦ | |||