:MEASure:LTESt:MLIMit:WAVeforms?
Query Syntax
:MEASure:LTESt:MLIMit:WAVeforms?
{1:16} identifies a Limit Line Test.
Description
Queries the number of waveforms acquired during a measurement limit test. To query the number of failures recorded, use the :MEASure:LTESt:MLIMit:FAILures? query. Use the :LTESt:MEASure:MLIMit:STATe command to turn on a measurement limit test.
Requires FlexDCA revision A.04.00 and above.
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Flex.query(':STATus?')):
measurement = Flex.query('?')
If averaging is turned on (:ACQuire:AVERaging), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:ECOunt?) versus the number of measurement sweeps that have occurred (:COUNt?). The technique uses the :COUNt? common measurement query. For example,
if (Flex.query(':COUNt?') >= Flex.query(':ACQuire:ECOUNt?')):
measurement = Flex.query('?')
You can also use an acquisition limit lest to test that a number of waveform samples, or pattern acquisitions have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.
Common Measurement Child Queries
This command supports the use of the following common measurement queries: :LOCation?, :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.