:MEASure:OSCilloscope:USER:COMMents?

Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8

Query Syntax

:MEASure:OSCilloscope:USER{1:8}:COMMents?

Description

Returns the comment string for the selected user measurement. The comment string is defined in the measurement's XML definition file using the <Comments> tag. The comment string is limited in length to 512 characters.

Use the :MEASure:OSCilloscope:USER parent command to turn on the measurement and return the measured value.

Requires FlexDCA revision A.05.00 and above.