:MEASure:OSCilloscope:USER:NAME?
Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8
Query Syntax
:MEASure:OSCilloscope:USER{1:8}:NAME?
Description
For the selected Oscilloscope mode user measurement, returns the measurement name that is shown on Oscilloscope mode's User measurement tab. If an XML file was used to define the test, the test name is specified in the file's XML <Name> tag. If this tag is missing, or empty, or if the user measurement was defined directly from a Matlab (*.m) or Python (*.py) file, the abbreviation is derived from the XML, Matlab, or Python filename. The string is limited in length to 15 characters. If the measurement has not been created, an empty string is returned.
Use the :MEASure:OSCilloscope:USER parent command to turn on the measurement and return the measured value.
Requires FlexDCA revision A.05.00 and above.