:MEASure:OSCilloscope:USER:REGion

Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:TDR:USER{1:8}:REGion {DISPlay | REGion{1:8}}

Description

Selects a waveform measurement region over which to perform the user measurement. This allows you to restrict the measurement over a specific portion of the waveform over the X axis. Measurement regions are available in FlexDCA's Oscilloscope and TDR/TDT modes. Use the :MEASure:REGions:STATe command to turn on an configure measurement regions.

Requires FlexDCA revision A.05.00 and above.