:MEASure:OSCilloscope:USER:LSTatus?
Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8
Query Syntax
MEASure:OSCilloscope:USER:LSTatus?
Description
Returns the status of the loading of the XML configuration file (:MEASure:OSCilloscope:USER:CFILe command). Use the :REASon child command to return the reason for a failed load.
Use the :MEASure:OSCilloscope:USER parent command to turn on the measurement and return the measured value.
Requires FlexDCA revision A.05.00 and above.