:MEASure:OSCilloscope:VMINimum:REGion
Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:MEASure:OSCilloscope:VMINimum:REGion {DISPlay | REGion{1:8}}
Query Syntax
:MEASure:OSCilloscope:VMINimum:REGion?
Description
Select a time span over which the :VMINimum measurement is made.
- DISPlay
- The measurement is performed on the displayed portion of the waveform. This is the default selection.
- REGion{1:8}
- The measurement is performed across one of eight regions. Regions are defined using the
:MEASure:REGions:STATecommand.
Example Command Sequence
:SYSTem:MODE OSCilloscope :MEASure:OSCilloscope:VMINimum:SOURce CHAN2A :MEASure:OSCilloscope:VMINimum:REGion REGion3 :MEASure:OSCilloscope:VMINimum :MEASure:OSCilloscope:VMINimum?