:MEASure:OSCilloscope:VMIDdle

Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:OSCilloscope:VMIDdle

Query Syntax

:MEASure:OSCilloscope:VMIDdle?

Description

Moves the Amplitude-at-Middle measurement to the top of the Results table. This measurement may be compatible with PAM4 signals, depending on the PAM4 waveform. Displays the measurement if it is not already shown on the table. The query form of the command returns the measured value. Amplitude-at-Middle is the measure of the amplitude value of the middle threshold. An annotation is placed on the display at the measured value. By default, this is the standard IEEE 50% threshold measurement level definition. The middle threshold value can be set to 50% or a custom value. The Waveform Base and Waveform Top are first located and these values are used to determine the threshold value. Sources can be any displayed waveform, waveform memory, or function. For example, CHAN1A, WMEMory1, or FUNCtion1. Use :MEASure:TBASe:METHod to change the definition of the waveform's top/base. Use :MEASure:THReshold:METHod to change the definition of the waveform's threshold.

PAM4 Compatibility. Because this measurement is based on waveform top and base levels and the passing of the waveform's edge through proximal, mesial, and distal thresholds, the measurement is not designed for PAM4 signals. However, the measurement may be able to be made on PAM4 signals if the waveform top and base definitions are manual set. This can be attempted using the following commands: :MEASure:TBASe:METHOd, :CHANnel:UDEFined:TOP, and :CHANnel:UDEFined:BASe commands.

Measurement Ready?

To confirm that the measurement is ready to read, you can query the measurement's status:

if ('CORR' in Flex.query(':MEASure:OSCilloscope:VMIDdle:STATus?')):
	measurement = Flex.query(':MEASure:OSCilloscope:VMIDdle?')

If averaging is turned on (:ACQuire:AVERaging), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:ECOunt?) versus the number of measurement sweeps that have occurred (:MEASure:OSCilloscope:VMIDdle:COUNt?). The technique uses the :COUNt? common measurement query. For example,

if (Flex.query(':MEASure:OSCilloscope:VMIDdle:COUNt?') >= Flex.query(':ACQuire:ECOUNt?')):
	measurement = Flex.query(':MEASure:OSCilloscope:VMIDdle?')

You can also use an acquisition limit lest to test that a number of waveform samples, or pattern acquisitions have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.

Common Measurement Child Queries

This command supports the use of the following common measurement queries: :LOCation?, :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.

Measurement Identification

Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.

For example, to return the status of the measurement, :MEASure:OSCilloscope:VMIDdle

flex.write(':MEASure:OSCilloscope:VMIDdle:SOURce CHAN1A')
if flex.query(':MEASure:OSCilloscope:VMIDdle:STATus?') == 'CORR';
    measurement = flex.query(':MEASure:OSCilloscope:VMIDdle?')
else:
	details = flex.query(':MEASure:OSCilloscope:VMIDdle:STATus:DETails?')
	reason = flex.query(':MEASure:OSCilloscope:VMIDdle:STATus:REASon?')

Child commands for measurement identification:

  • :MEASure:OSCilloscope:VMIDdle:SOURce
  • :MEASure:OSCilloscope:VMIDdle:REGion

Example Command Sequence

:SYSTem:MODE OSCilloscope
:MEASure:OSCilloscope:VMIDdle:SOURce CHAN1A
:MEASure:OSCilloscope:VMIDdle
:MEASure:OSCilloscope:VMIDdle?