:MEASure:PLEVel:ISI
Command Syntax
:MEASure:PLEVel:ISI
Query Syntax
:MEASure:PLEVel:ISI?
Description
For a PAM4 waveform, displays a Inter-Symbol Interference (ISI) measurement in the Level table. If the measurement is already listed, the measurement is moved to the top of the table. Use the query form of the command to return the measured value. The measurement is made at the signal logic level that is specified with the :MEASure:PLEVel:ISI:LEVel child command.
| Select | Command |
|---|---|
| Signal logic level | :MEASure:PLEVel:ISI:LEVel
|
| Level definition (average or minimum number of consecutive identical digits, CID) | :MEASure:AMPLitude:DEFine:LEVel
|
| Units (current noise / interference units) | :MEASure:AMPLitude:DEFine:UNITs
|
Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.
Measurement Identification
Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.
For example, to return the status of the measurement, :MEASure:PLEVel:ISI
flex.write(':MEASure:PLEVel:ISI:SOURce CHAN1A')
if flex.query(':MEASure:PLEVel:ISI:STATus?') == 'CORR';
measurement = flex.query(':MEASure:PLEVel:ISI?')
else:
details = flex.query(':MEASure:PLEVel:ISI:STATus:DETails?')
reason = flex.query(':MEASure:PLEVel:ISI:STATus:REASon?')
Child commands for measurement identification:
:MEASure:PLEVel:ISI:SOURce
Requires FlexDCA revision A.06.00 and above.
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Flex.query(':MEASure:PLEVel:ISI:STATus?')):
measurement = Flex.query(':MEASure:PLEVel:ISI?')
If averaging is turned on (:ACQuire:AVERaging), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:ECOunt?) versus the number of measurement sweeps that have occurred (:MEASure:PLEVel:ISI:COUNt?). The technique uses the :COUNt? common measurement query. For example,
if (Flex.query(':MEASure:PLEVel:ISI:COUNt?') >= Flex.query(':ACQuire:ECOUNt?')):
measurement = Flex.query(':MEASure:PLEVel:ISI?')
You can also use an acquisition limit lest to test that a number of waveform samples, or pattern acquisitions have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.
Common Measurement Child Queries
This command supports the use of the following common measurement queries: :LOCation?, :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.