:MEASure:PLEVel:LIST:CLEar
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Level
Command Syntax
:MEASure:PLEVel:LIST:CLEar
Description
Clears the entire active PAM measurement list in the displayed Level results table.
Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.
Requires FlexDCA revision A.06.00 and above.
Example Command Sequence
:SYSTem:MODE JITTer :MEASure:AMPLitude:DEFine:ANALysis ON :MEASure:PLEVel:LIST:CLEar