:MEASure:PLEVel:LIST:DEFault
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Level
Command Syntax
:MEASure:PLEVel:LIST:DEFault
Description
Resets the Level results table to show the default active PAM4 measurement list in the table.
Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.
Requires FlexDCA revision A.06.00 and above.
Example Command Sequence
:SYSTem:MODE JITTer :MEASure:AMPLitude:DEFine:ANALysis ON :MEASure:PLEVel:LIST:DEFault