:MEASure:PLEVel:LIST:SELect

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Level

Command Syntax

:MEASure:PLEVel:LIST:SELect <row_index>, <column_index>

<row_index> is an int starting at 1 for the first data row. <column_index> is an int and, although required, it is ignored.

Query Syntax

:MEASure:PLEVel:LIST:SELect?

Description

In Jiter Mode's Level panel for PAM4 Level measurements, selects a Level measurement row in the panel's table. The arguments are two comma-separated integers that represent the table row and column. However, only the row argument is used. The column argument is ignored, but must be supplied. The recommended column index should be 0. Data rows can be specified and selected but not the table heading row. The top measurement is identified as 1,0. For example, in the following figure the highlighted row was selected by sending 4,0. To remove an entire measurement row from the table, use the :MEASure:PEYE:LIST:REMove command.

Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.

Requires FlexDCA revision A.05.60 and above.