:TRACe:UDEFined:BASe
Command Syntax
:TRACe{1:128}:UDEFined:BASe <amplitude>
Where the {1:128} specifier identifies a trace.
Where the <amplitude> argument is a double.
Query Syntax
:TRACe{1:128}:UDEFined:BASe?
Description
For the indicated T-domain parameter or S-parameter trace, sets or queries the custom base-level setting. The top and base levels are used to locate a waveform's lower, middle, and upper threshold levels during measurements. Specify the level in the units shown in the following table, depending on the waveform type. Use :TRACe:UDEFined:TOP to set or query a custom top level. Before this custom base level can be applied to measurements, use the :MEASure:TBASe:METHod command to select custom top-base definitions. This setting can be set from the front panel by clicking Measure > Configure Base Measurements and selecting in the Top-Base Definition tab in the Configure Measurements dialog.
| Content Window Graphs | Y-Axis Units |
|---|---|
| T-Domain Parameters | |
| Time-Ohms | Ohms |
| Time-Volts | Volts |
| Time-% | Percent |
| S-Parameters | |
| Freq-Mag | Decibels |
| Phase | Degrees |
| GrpDelay | Seconds |
Requires FlexDCA revision A.04.00 and above.
Example Command
:TRACe2:UDEFined:BASe 2.0E-1