:MTESt:DISPlay
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MTESt{1:16}:DISPlay {ON | OFF | 1 | 0}
Where the {1:16} specifier identifies a specific mask.
Query Syntax
:MTESt{1:16}:DISPlay?
Query Response
{1 | 0}
Description
Turns the mask testing on or off. When a mask is loaded (:MTESt:LOAD), the mask is automatically displayed. When a mask is turned off, the mask remains loaded in FlexDCA and you can simply display the mask again without having to re-load it. Performing a default setup (:SYSTem:DEFault) unloads the mask.
Example Command Sequence
:MTESt2:LOAD:FNAMe "009.95328 - 10GbE_9_953_May02.mskx" :MTESt2:LOAD … … :MTESt2:DISPlay OFF … … :MTESt2:DISPlay ON