:MTESt:SOURce
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MTESt{1:16}:SOURce <source_waveform>
Where the {1:16} specifier identifies a specific mask.
Where <source_waveform> can be one of the following:
CHANnel{1:8}{A|B|C|D}CGMemory{1:8}FUNCtion{1:16}
Query Syntax
:MTESt{1:16}:SOURce?
Description
Selects the source waveform when more than one source is displayed.