:MTESt:MLOaded?
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Where the {1:16} specifier identifies a specific mask.
Query Syntax
:MTESt{1:16}:MLOaded?
Description
Queries whether a mask has been loaded. Masks are loaded using the :MTESt:LOAD command. When mask testing is turned off using the :MTESt:DISPlay OFF command, the mask is still loaded in FlexDCA and this query returns true.