:MTESt:MARGin:AUTo:HITs
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MTESt{1:16}:MARGin:AUTo:HITs <hits>
<hits> is an integer.
Where the {1:16} specifier identifies a specific mask.
Query Syntax
:MTESt{1:16}:MARGin:AUTo:HITs?
Description
Automatically sets the margin size based on a target hit count. The margin is sized so that:
Automatic margin sizing can also be based on a hit ratio as determined by the :MTESt:MARGin:AUTo:METHod command.
Example Command Sequence
:MTESt3:MARGin:METHod AUTO :MTESt3:MARGin:AUTo:METHod HITS :MTESt3:MARGin:AUTo:HITs 10 :MTESt3:MARGin:STATe ON :MTESt3:LOAD:FNAMe "009.95328 - 10GbE_9_953_May02.mskx" :MTESt3:LOAD