:MTESt:MARGin:METHod
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MTESt{1:16}:MARGin:METHod {MANual | AUTO}
Where the {1:16} specifier identifies a specific mask.
Query Syntax
:MTESt{1:16}:MARGin:METHod?
Description
Selects the manual or automatic method of setting the margin size.
- MANual
- Selects manual margin configuration where the margin size is configured as a percentage of the mask. Use the
:MTESt:MARGin:PERCentcommand to enter the margin size as a percentage of the mask. - AUTO
- Selects automatic margin configuration where the margin size is configured based on a target hit count or target hit ratio. Use the
:MTESt:MARGin:AUTo:METHodcommand to select between hit count or hit ratio.