:MTESt:MARGin:AUTo:METHod
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MTESt{1:16}:MARGin:AUTo:METHod {HITS | HRATio}
Where the {1:16} specifier identifies a specific mask.
Query Syntax
:MTESt{1:16}:MARGin:AUTo:METHod?
Description
Selects that automatic configuration of the margin size is to be based on a target hit count (HITS) or target hit ratio (HRATio). Automatic mask margin configuration must first be enabled using the :MTESt:MARGin:METHod command.
Example Command Sequence
:MTESt2:MARGin:METHod AUTO :MTESt2:MARGin:AUTo:METHod HITS :MTESt2:MARGin:AUTo:HITs 10 :MTESt2:MARGin:STATe ON :MTESt2:LOAD:FNAMe "009.95328 - 10GbE_9_953_May02.mskx" :MTESt2:LOAD