:REPository:MEASure:PUBLish:ULIMit
Meas. mode:
Scope
Eye
Jitter
TDR
Publish mode:
Custom
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:REPository:MEASure:PUBLishN:ULIMit
Where N identifies a custom measurement and must be a value from 1 to 16 {1:16}. For example, :REPository:MEASure:PUBLish2:ULIMit
.
Query Syntax
:REPository:MEASure:PUBLishN:ULIMit?
Description
For the Custom publishing mode, sets an upper limit beyond which the measurement result will not be published.
Requires FlexDCA revision A.05.70 and above.
Starting with FlexDCA revision A.06.02, a FlexDCA license is no longer required to use FlexDCA with the N8844A Data Analytics Web Service Software.
Example Command Sequence
FlexDCA.write(':REPository:MEASure:PMODe CUSTom') index = FlexDCA.query(':MEASure:EYE:RISetime:LOCation?') FlexDCA.write(':REPository:MEASure:PUBLish2:SOURce:TYPE EYE') FlexDCA.write(':REPository:MEASure:PUBLish2:SOURce:LOCation ' + index) FlexDCA.write(':REPository:MEASure:PUBLish2:NAME "Rise Time at 38C"') FlexDCA.write(':REPository:MEASure:PUBLish2:ULIMit 30.0E-12') FlexDCA.write(':REPository:MEASure:PUBLish2:LLIMit 20.0E-12') FlexDCA.write(':REPository:MEASure:PUBLish2:STATe ON') FlexDCA.query(':REPository:PUBLish;*OPC?')