:REPository:MEASure:PMODe
Command Syntax
:REPository:MEASure:PMODe {SELected | CUSTom}
Query Syntax
:REPository:MEASure:PMODe?
Query Response
{SEL | CUST}
Description
Selects one of two methods that can be used to select the measurements to publish. The two publishing modes have different features as shown in the following table:
Ability to… | Publishing Mode | |
---|---|---|
Selected | Custom | |
Select single measurements | ♦ | ♦ |
Quickly select all measurements | ♦ | |
Quickly clear all measurements | ♦ | |
Assign a custom name to a measurement | ♦ | |
Set upper and lower measurement limits | ♦ | |
Publish up to the number of displayed measurements | ♦ | |
Limited to 16 measurements | ♦ |
SELected Mode
When using Selected publishing mode, measurements are selected without any options. This is equivalent to the fields shown in the following picture of the Repository Setup dialog. Use the command that are listed in the following two tables to select measurements for publishing. The first table lists commands for selecting specific measurements. The second table lists commands that select or clear all measurements in displayed results panel. Selecting all measurements is faster and easier than selecting individual measurement because it does not require the use of indexes to select each measurement.
Measurements that are not active (displayed in a table) cannot be selected.
CUSTom Mode
When using Custom publishing mode, up to 16 measurements can be selected with the ability to define upper and lower measurement limits and to give custom name the custom bounded measurement. This is equivalent to the fields shown in the following picture of the Repository Setup dialog.
Use the following commands to configure Custom publishing mode.
Measurements that are not active (displayed in a table) cannot be selected.
- :REPository:MEASure:PUBLish:NAME
- :REPository:MEASure:PUBLish:LLIMit
- :REPository:MEASure:PUBLish:SOURce:LOCation
- :REPository:MEASure:PUBLish:SOURce:TYPE
- :REPository:MEASure:PUBLish:STATe
- :REPository:MEASure:PUBLish:ULIMit
Requires FlexDCA revision A.05.70 and above.
Starting with FlexDCA revision A.06.02, a FlexDCA license is no longer required to use FlexDCA with the N8844A Data Analytics Web Service Software.