:SLOT:SWITch:ROUTe:LIST?

Instruments:
Switch
Flex Apps:
FlexDCA
Package License:
L-RND
L-MFG

Query Syntax

:SLOT{1:8}:SWITch:ROUTe:LIST? ["<switch-ID>"]

Where the {1:8} specifier identifies a module slot.

Where <switch-ID> is an optional parameter that identifies a switch on switch products that have multiple internal optical switches. If the device does not have multiple switches, this parameter should not be used.

Description

Returns a comma separated string of all switch ports. The following table lists examples of possible strings returned from supported modules.

Examples of Returned Switch Ports
Switch Example Switch ID1 Examples of Returned Port Strings
Keysight N7731A Switch 1 "A, 1, 2, 3, 4"
Switch 2 "A, 1, 2, 3, 4"
Keysight N7734A — "A, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13"
DiCon GP750 SL1:M1 "IN, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12"
SL2:M1 "IN, 1, 2"
SL2:M2 "IN, 1, 2"
SL2:M3 "IN, 1, 2"
SL3:X1 "IN 1, IN 2, IN 3, IN 4, IN 5, IN 6, IN 7, IN 8, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, 16, 17, 18, 19, 20, 21, 22, 23, 24, 25, 26, 27, 28, 29, 30, 31, 32"
DiCon GP600 — "IN, 1, 2, 3, 4, 5, 6, 7, 8"
— "IN 1, IN 2, IN 3, IN 4, IN 5, IN 6, IN 7, IN 8, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, 16, 17, 18, 19, 20, 21, 22, 23, 24, 25, 26, 27, 28, 29, 30, 31, 32"
Polatis 6000 Ultra Switch — "1, 2, 3, ... , 46, 47, 48"

If switch includes multiple switches.

Requires FlexDCA revision A.07.00 and above.