:SLOT:SWITch:VERify:CHANnel
Instruments:
Switch
Flex Apps:
FlexDCA
Package License:
L-RND
L-MFG
Command Syntax
:SLOT:SWITch:VERify:CHANnel
Query Syntax
:SLOT:SWITch:VERify:CHANnel?
Description
Specifies the receiver module (DCA-X or DCA-M) input channel that is used to measure the signal on the switch's output.
Requires FlexDCA revision A.07.00 and above.
Example Command Sequence
code here!