:SLOT:SWITch:WAVelength

Instruments:
Switch
Flex Apps:
FlexDCA
Package License:
L-RND
L-MFG

Command Syntax

:SLOT:SWITch:WAVelength {WAVelength{1:5} | UNSPecified}

Where the {1:8} specifier identifies a module slot.

Where the argument WAVelength{1:5} selects a wavelength setting.

Query Response

{WAV1 | WAV2 | WAV3 | WAV4 | WAV5 | UNSP}

Description

For an optical switch that includes an internal tunable optical filter, selects the wavelength setting. The following table lists the optical switches that support wavelength selection. If the switch does not support wavelength selection, the query form of this command returns UNSP, which is short for UNSPecified.

Switches that Support the Wavelength Setting
Switch Wavelength
Setting
Keysight N7734A-009 —
Keysight N7731C-009 —
Dicon GP750 ●1
Dicon GP600 ●1
Polatis Series 6000 ultra switch

Always confirm the ability of a the switch to accept a wavelength setting and what selections are available. Your switch model/option may or may not include internal tunable optical filters.

Requires FlexDCA revision A.07.00 and above.