:SPRocess:DDEConvolve:BLIMit

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND

Command Syntax

:SPRocessN:DEConvolve:BLIMit {NONE | GAUSsian | SINC}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:DDEConvolve:BLIMit?

Description

Specifies the type of bandwidth filter used in a Remove s4p operator. Use the :SPRocess:DDEConvolve:BANDwidth command to specify the function's bandwidth. Use the :SPRocess:DDEConvolve:FNAMe command to open an existing network file that models your test setup.

NONE
No filter is applied.
GAUSsian
A Gaussian filter is used, which is the default.
SINC
Selects a sin(x)/x filter.

Example Command Sequence

:FUNCtion2:FOPerator DDEConvolve
:SPRocess2:DDEConvolve:FNAMe "C:\Users<user_name>\Documents\Keysight\FlexDCA\S-Parameter Data\DUT_4.s4p"
:SPRocess2:DDEConvolve:FMODel ON  // Flips  S-parameters ports
:SPRocess2:DDEConvolve:BANDwidth:AUTo OFF
:SPRocess2:DDEConvolve:BANDwidth:BLIMit GAUSsian
:SPRocess2:DDEConvolve:BANDwidth 7.5E9
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.