:SPRocess:DDEConvolve:FMODel

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND

Command Syntax

:SPRocessN:DDEConvolve:FMODel {ON | OFF | 1 | 0}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocess{1:16}DDEConvolve:FMODel?

Query Response

{1 | 0}

Description

Flips the S-parameters for an Remove s4p operator. If S-parameter file's data is not defined with the ports located as shown in the top two diagrams in the following table, flip the S-parameters to ensure that the S-parameter order is properly interpreted. Use the :SPRocess:DDEConvolve:PORDer command to ensure that the S-parameter port order is also properly interpreted.

Arguments and Dialog Settings for 4-Port S-Parameters Files
Port Configuration in File Flip Model Argument
(DDEConvolve:FMODel)
4 Port Numbering Argument
(:DDEConvolve:PORDer)
OFF
PORDer1324
OFF
PORDer1234
ON
PORDer1324
ON
PORDer1234

Example Command Sequence

:FUNCtion2:FOPerator DDEConvolve
:SPRocess2:DDEConvolve:FNAMe "C:\Users<user_name>\Documents\Keysight\FlexDCA\S-Parameter Data\DUT_4.s2p"
:SPRocess2:DDEConvolve:FMODel ON  // Flips  S-parameters ports
:SPRocess2:DDEConvolve:PORDer PORDer1324
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.