:SPRocess:DEConvolve:FMODel

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND

Command Syntax

:SPRocessN:DEConvolve:FMODel {ON | OFF | 1 | 0}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocess{1:16}DEConvolve:FMODel?

Query Response

{1 | 0}

Description

Flips the S-parameters input to a Remove s2p operator. If S-parameter file's data is not defined with the ports located as shown in the following diagram, flip the S-parameters to ensure that the S-parameter order is properly interpreted.

Example Command Sequence

:FUNCtion2:FOPerator DEConvolve
:SPRocess2:DEConvolve:FNAMe "C:\Users<user_name>\Documents\Keysight\FlexDCA\S-Parameter Data\DUT_4.s2p"
:SPRocess2:DEConvolve:FMODel ON  // Flips  S-parameters ports
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.