:SPRocess:DEConvolve:MGAin
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Command Syntax
:SPRocess{1:64}:DEConvolve:MGAin <maximum-gain>
Where {1:64} identifies one of up to 64 possible operators that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Where <maximum-gain> is a float. For example, 20.0.
Query Syntax
:SPRocess{1:64}:DEConvolve:MGAin?
Query Response
<maximum-gain>
Description
Sets the Remove s2p operator's maximum gain. The default value is 2.0E+01. The minimum value is 0E+00. The maximum value is 1.00E+02.
Requires FlexDCA revision A.07.90 and above.
Example Command
:SPRocess5:DEConvolve:MGAin 2.0E+01