:SPRocess:FFT:NFRequency
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
TDR
Package License:
L-RND
Command Syntax
:SPRocessN:FFT:NFRequency <double>
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Where <double> is the FFT normalization frequency. For example, 1.00E+5.
Query Syntax
:SPRocessN:FFT:NFRequency?
Description
Sets the FFT normalization frequency when the FFT's display is set to dB (Normalized) using the :SPRocess:FFT:DISPlay command. The default value is 0 Hz. The minimum value is 0 Hz. The maximum value is 500 GHz.
Requires FlexDCA revision A.05.80 and above.