:SPRocess:FFT:WINDow

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
TDR
Package License:
L-RND

Command Syntax

:SPRocess{1:64}FFT:WINDow {NONE | HANNing}

Where N identifies one of up to 64 possible operators {1:16} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:FFT:WINDow?

Description

Turns on or off the application of a Hanning shaping window to an FFT operator.

Example Command Sequence

:FUNCtion2:FOPerator FFT
:SPRocess2:FFT:DISPlay DBM
:SPRocess2:FFT:WINDow HANNing
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.