:SPRocess:FFT:DISPlay

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
TDR
Package License:
L-RND

Specifies the output format of an FFT operator to be one of the types listed below. When phase (PHASe), unwrapped phase (UPHase), or group delay (GDELay) is selected, use the :FFT:PREFerence command to set the FFT phase reference to left, center, or manual. If you select manual, use the :FFT:PREFerence:TORigin command to enter the FFT origin in seconds. If the input is an optical signal and dBV (Electrical) is selected, use the :FFT:TFACtor command to enter the voltage conversion factor (V/W).

  • Linear Magnitude (MAGNitude)
  • dBV (DBV)
  • dBm (DBM)
  • Phase (PHASe)
  • Unwrapped Phase (UPHase)
  • Group Delay (GDELay)

To ensure that enough data is available to construct a useful FFT, set FlexDCA's timebase scale equal to the waveform's period. This will display 10 waveform cycles. For example, for a 5 GHz (200 ps) reference clock, enter a scale setting of 200 ps/division.

Content Windows

The FFT waveform is automatically displayed in the appropriate type of content window, which is listed in the following table and displayed in the above picture. For the MAGNitude, PHASe, and GDELay arguments, you can optionally move the waveform to an additional content window of the same type using the :FUNCtion{1:64}:CWINDdow command. For example,

:FUNCtion1:FOPerator FFT  // Create an FFT function.
:FUNCtion1:OPERand1 CHAN1A  // Assign input waveform.
:SPRocess1:FFT:DISPlay GDELay  // Select output waveform type. Waveform is automatically assigned to content window GDELay1. 
:FUNCtion1:CWINdow GDELay2  // Display content window GDELay2 (Delay 2) and re-assign output waveform from GDELay1 to GDELay2.

When MAGNitude is selected, the waveform is displayed in a Waveform waveform content window. To view the FFT waveform, turn on pattern lock (:TRIGger:PLOCk ON) so that a single-valued waveform is provided as the function's input. In Eye mode, if the entire pattern is acquired (:ACQuire:EPATtern ON), additionally turn waveform wrapping off (:ACQuire:WRAPping OFF).

Command Arguments and Resulting Waveform Content Window
Argument Equivalent
GUI Selection
Displayed
Content Window
Number of
Available Windows
Scale Units
Via
Front Panel
Programmatically
MAGNitude Linear Magnitude Waveform 1 1 Y-Axis: Volts or Watts (linear scale)
X-Axis: seconds
DBV dBV Magnitude 1 4 Y-Axis: dB (logarithmic scale)
X-Axis: Hertz
DBM dBm
PHASe Phase Phase 1 4 Y-Axis: phase (°)
X-Axis: Hertz
UPHASe Unwrapped Phase
GDELay Group Delay Delay 1 4 Y-Axis: seconds
X-Axis: Hertz

The ability to use waveform content windows was added starting with FlexDCA revision A.03.00.

Example Command Sequence

:FUNCtion2:FOPerator FFT
:SPRocess2:FFT:DISPlay DBM
:SPRocess2:FFT:WINDow HANNing
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.