:SPRocess:PFIT:DELay
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Package License:
L-RND
Command Syntax
:SPRocessN::PFIT:DELay <unit-intervals>
<unit-intervals> is an integer.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN::PFIT:DELay?
Description
For a a Pulse Fit filter operator, specifies the Pulse Delay (Dp) which is the number of precursor Unit Intervals (UIs) to include in the algorithm to ensure that a portion of the pulse's rising edge is captured. The default value is 3 UI. The minimum setting is 1 UI. The maximum setting is 10 UI. of a Pulse Fit filter operator. To select the filter's display mode, use the :SPRocess:PFIT:DISPlay command.
Requires FlexDCA revision A.07.50 and above.
Example Command Sequence
:FUNCtion2:FOPerator PFIT :SPRocess2:PFIT:DISPlay PRESponse :SPRocess2:PFIT:DELay 3 :SPRocess2:PFIT:LENGth 200 :SPRocess2:PFIT:ZPAD OFF :FUNCtion2:DISPlay ON