:SPRocess:PFIT:LENGth
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SPRocessN:PFIT:LENGth <unit-intervals>
<unit-intervals> is an integer.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:PFIT:LENGth?
Description
For a Pulse Fit filter operator (:FUNCtion:FOPerator PFIT
), specifies the Pulse Length (Np) sets the duration to be used when modeling the pulse response. This is the maximum extent that can exist for a single pulse. The default value is 200 UI. The minimum setting is 9 UI. The maximum setting is 1,000 UI.
Requires FlexDCA revision A.07.50 and above.
Example Command Sequence
:FUNCtion2:FOPerator PFIT :SPRocess2:PFIT:DISPlay PRESponse :SPRocess2:PFIT:DELay 3 :SPRocess2:PFIT:LENGth 200 :SPRocess2:PFIT:ZPAD OFF :FUNCtion2:DISPlay ON