:SPRocess:PFIT:ZPAD
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SPRocessN:PFIT:ZPAD {ON | OFF}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:PFIT:ZPAD?
Description
For a Pulse Fit filter operator (:FUNCtion:FOPerator PFIT
), specifies the Zero-Pad Output for Signal Processing. Use this setting in cases where the response waveform goes beyond the Pulse Length. Zero level values are added. By default, this setting is cleared.
Requires FlexDCA revision A.07.50 and above.
Example Command Sequence
:FUNCtion2:FOPerator PFIT :SPRocess2:PFIT:DISPlay PRESponse :SPRocess2:PFIT:DELay 3 :SPRocess2:PFIT:LENGth 200 :SPRocess2:PFIT:ZPAD OFF :FUNCtion2:DISPlay ON