:SPRocess:RCOSine:FSTart
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:SPRocessN:RCOSine:FSTart <start_frequency>
<start_frequency> is a double.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:RCOSine:FSTart?
Description
Specifies the start frequency in Hertz of a raised cosine filter operator. To specify the end frequency, use the :SPRocess:RCOSine:FEND command. To configure the filter's Aliased Noise Processing, use the :SPRocess:RCOSine:PNOise command.
Requires FlexDCA revision A.07.40 or greater.
Example Command Sequence
:FUNCtion2:FOPerator RCOSine :SPRocess2:RCOSine:FSTart 5.40E10 :SPRocess2:RCOSine:FEND 7.50E10 :FUNCtion2:COLor TCOLor4 :FUNCtion2:DISPlay ON *OPC?