:SPRocess:USER:CFILe:RELoad
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
TDR
Package License:
L-RND
Command Syntax
:SPRocessN:USER:CFILe:RELoad
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Description
Reloads the XML configuration file for the selected user-defined function.
Use the :SPRocess{1:16}:USER:CFILe parent command to configure the function.
Requires FlexDCA revision A.05.00 and above.