:SPRocess:USER:CONTrol:FILE
Command Syntax
:SPRocessN:USER:CONTrol{1:4}:FILE <file_name>
<file_name> is a string that includes the file name and any path.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:USER:CONTrol{1:4}:FILE?
Description
Sets the value of a function's user-defined control which has been configured as a file. User-defined controls are shown in the function's User Operator Setup dialog. The controls are numbered 1 to a maximum of 4 starting with the top control shown in the dialog. For example, the following figure shows how two controls are numbered:
- "N", an integer, is control 1.
- "Test File", a file, is control 2.
Since control 2 is defined as a file, you could set its value to "data.txt" using the following command:
SPRocess1:USER:CONTrol2:FILE "data.txt"
In this case, the sibling commands DOUBle, ENUM, INTeger, and STRing do not affect this user-defined control as the control has been defined as an string in the XML configuration file. The query form of the command returns current value of the user-defined control.
Use the :SPRocess{1:16}:USER:CFILe command to load the XML configuration file for the function.
Requires FlexDCA revision A.05.00 and above.