:TRACe:UDEFined:DISTal
Command Syntax
:TRACe{1:128}:UDEFined:DISTal <amplitude>
Where the {1:128} specifier identifies a trace.
Where the <amplitude> argument is a double.
Query Syntax
:TRACe{1:128}:UDEFined:DISTal?
Description
For the indicated T-domain parameter or S-parameter trace, sets or queries the custom upper-threshold definition level. This command is used when making measurements with custom threshold definitions that are based on absolute amplitude. Before using this command,
- Use the
:MEASure:THReshold:METHodcommand to specify the use of custom threshold definitions. - Use the
:MEASure:THReshold:UNITscommand to specify absolute amplitude threshold definitions. When custom threshold definitions are based on percent, use the:MEASure:THReshold:MESialcommand instead.
Use the :TRACe:UDEFined:MESial command to enter a middle threshold level. Use the :TRACe:UDEFined:PROXimal command to enter a lower threshold level.
The custom upper-threshold setting can be set from the front panel by clicking Measure > Configure Base Measurements and selecting the Thresholds tab in the Configure Measurements dialog.
Depending on the waveform type, specify the level in the units shown in the following table.
| Content Window Graphs | Y-Axis Units |
|---|---|
| T-Domain Parameters | |
| Time-Ohms | Ohms |
| Time-Volts | Volts |
| Time-% | Percent |
| S-Parameters | |
| Freq-Mag | Decibels |
| Phase | Degrees |
| GrpDelay | Seconds |
Requires FlexDCA revision A.04.00 and above.
Example Command
:TRACe2:UDEFined:DISTal 7.4E-1